Hi teams
The output voltage of TPS61020 becomes the same potential as the input voltage. Although the set voltage is set to 3.05 V and the enable pin is pulled up to the power supply voltage, the input voltage is output as it is without being boosted. The voltage at the FB pin is 0.35V, so it should work, but it does not work.
Please let me know what is the reason for this. Best regards Hayashi