Other Parts Discussed in Thread: PMP40328, UCC27712, UCC21220A, TIDA-00173, ISO7740, ISO7720, LMG1020, UCC27511, UCD3138
Hi
It is strictly not an LM5114 question. Related.
Pl see attached "GaN power switch Stack" for a bridgeless ac-dc converter in fixed freq. resonant mode.
The node where the sine wave is shown can go as high as 1100V with max line input( wrt to local neutral).
For many practical reasons, we have to use GaN parts. But there is no other way than stacking to switch bipolar voltage with this limit of +1100V/-100V waveform at switching rate( 150 kHz)
Is there any clever way to avoid so many floating gate drives?....like your "cascode" for the HV input low power converter using UCC287xx series?