Other Parts Discussed in Thread: UCD3138
Hi,
Why do not use bead to connect between V33A and V33D ?
is there any issue ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Why do not use bead to connect between V33A and V33D ?
is there any issue ?
A resistor between V33A and V33D together with the capacitor acts as a low pass filter to clean the voltage on V33A further.
Bead can cause instability, therefore should not be used.
Too small of resistor will not be effective enough in filtering.
Too big of a resistor can cause too much of drop in V33A due to current going through and cause premature reset.
Resistor values between 1 Ohms to 3 Ohms are good.
Regards,
Hi Yitzhak Bolurian
Why does bead cause instability?
Review some paper include TI C2000 and Microchip, it suggested using bead.
Why is UCD3138 different from the others? How to prove the use of resistor is better?
The internal circuitry is different in each device/chip, therefore the need for different external components to support proper functionality.
This is quite similar to the need for different type of engine oil or fuel in different cars.
The resistor as mentioned in the UCD3138 guideline is matching the proper functionality of UCD3138.
If the above answers your question, please set the status of this post to resolved.
Regards,