Hello,
I have a problem with the 2 event classification of the TPS23754 in combination with the PoE injector GT-96300-3656-T3-AP from Globtek. The injector is a 802.3at injector
but our device which contains the TPS23754 is detected as a 802.3af device. The indicator LED which is connected to Pin 20 is not illuminated. All other tested power supplies work properly together with our device. And the GT-96300-3656-T3-AP
works properly together with some other tested 802.3at devices. Threre is some kind of ripple at a frequency of
approximately 3.9kHz on the first classification event. The second one is missing. The evalutation module TPS23754EVM-383 does also not work together with the mentioned poe injector.
The oscillogram of the failed classification is as follows.
Normally the oscillogram should look like this
This is a part of the circuitry around the TPS23754 in our design.
Thanks for any help!