Iwoudl liekto ask the follwing questions:
From VIN =5V, Configuration "CombinedNegativeVoltageConversionandPositiveSupplyDoubling" dtasheet page 13 Figure 10
1) Is correct to assume in this configuration Vout+ = 10, Vout-=-10V ?
2) In the figure 10 -V= –(nV – Vdx) seems if VIN=5V , in this configuration -Vout = 5V ? IS correct ?
3) IS question 2 is corrrectassumption , the only way to have from VOUT+ =10V, Vout-=-10V from VIN = 5V , is to have two part in cascade ?
Regards
Albert