Other Parts Discussed in Thread: LMG1210, LM50
I need to design the following buck converter. The converter switches the load to 12V instead of the classical way to GND. (see photo)
This is because of the installation, orientation and polarized current flow requirements of the load.
I need a half bridge power stage with short circuit protection and temperature shut down for both Mosfets.
Can CSD96497Q5MC do it?. If not any recommendation for alternatives?
Converter:
Input Voltage: 12V
Output Voltage: Variable 0.5V..7V
Output current: Variable 0..25A
Switching frequency: any device between 100kHZ..2MHZ
Best regards.