Hi there,
We use TPS7A4901DRBR to convert 5V-->3.3V , 5V-->2.5V, 5V-->1.8V, and 5V.3-->5V.
Just to make sure: VREF is voltage measured at NR/SS pin, and it is 1.188V, with 1.176V~1.212V range. And VFB is 1.185V±2.5%. Is this understanding correct?
Why bother to give out these two value ? VREF seems to be useless in designing process.
I thought we all we need is to use VFB=1.185V±2.5% to calculate Vout's nominal and max, min value, and consider tolerance of R1 and R2 at the same time.
If I was wrong, pls point out. Thanks.