This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4040-N: LM4040BIM3-2.5/NOPB Output Voltage Tolerance question

Part Number: LM4040-N

Hi Ti team,

       We test LM4040BIM3-2.5 Output Voltage Tolerance outside 0.2% in Ta=20°C to 23°C, test output Vref is 2.51V or 2.513V

SCH as below,

       Could you pls help us check that does IC failed or below SCH design probem or test method problem? thanks!