Part Number: BQ76940
Other Parts Discussed in Thread: BQ78350
Hello,
we developed a 13s BMS with the bq76940 and the companion IC bq78350.
The companion IC is managing the balancing.
In an big field test we have the problem, that on nearly 1/3 of 100 BMS the most upper balancing resistor is defective (burned away from overstress). This was discovered, when deeply discharged batteries (2,7V-3V) stand for some days and couldnt be charged anymore. The check of the cellvoltages showed, that one of 13 cells was deeply discharged (<1V), the rest had 2,7V-3V. Most of the time was the deep discharged cell the most upper cell, where the balancing resistor is defective. The balancing Mosfet is ok. The resistor is a thick film resistor with 0,5W an 47R.
Do you have any idea why the cells have been discharged and the resistor gets broken?