Other Parts Discussed in Thread: TIDA-00161
Dear TI experts,
I am currently designing driver for 96 x 96 pixel LED matrix using TLC59581 for my company, and the design is based on TIDA-00161. There will be several boards manufactured, thus I have to make sure that there is no loose ends. I found more documentation on the application user guide :
TLC58581 application user guide with Novastar software.ppt
I would like to request for more detailed documentation for this if possible, because there are several things that I am not yet very sure :
1. For 5 multiplexing through decoder, I found that signal E is using data pin from the receiver card, I would like to know if there is any particular reason to use data32 for signal E ?
2. Could the data output be configured ? e.g. for D1 in the driver, the data comes from data4 or data5 from the receiver card.
3. In TIDA-00161, it mentioned the use of readback function, how is the interface configured for this case ? Is it connecting D1_back, D2_back to any of the data pins from the receiver card ?
4. Is the SCLK_back necessary to use the readback function ?
Thank you and looking forward to your reply.
Regards,
Reno