Before very closing to battery fully charged, everything is normal. But once the battery fully charged, the battery voltage gets fluctuation. It is about 12.06 to 12.56V jump. The STAT also starts blinking. At this time, if drain the battery and turn off the board quickly. The battery voltage gets stable to about 12.5V.
It is same, no matter if turn/off the load of bq24133. The strange thing is the battery voltage is still fluctuation even the external power removed. Just the fluctuation amplitude gets smaller in this case.