This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161-Q1: The Inductor ripple current

Part Number: LM5161-Q1

Hello,

I need your help.Pleas

Which the inductor Ripple current do you recommend to me.


I have the following:

Vin,max=60V

Iout,max=0.5

Vout= 15 V

Thanks.