Other Parts Discussed in Thread: TPS54240-Q1
Hi Team,
One of my customer is using TPS54260-Q1 in below configuration.
Operating Range: 6V to 18V
Normal output voltage: 5V
Normal operating current: 1.0A(Max)
Sleep or light load current : 400 to 500uA
During light load conditions when the load current is 500uA and when input voltage is in the range of 6 to 6.5v, the Power Good signal is getting triggered by the regulator which in turn is causing system reset.
In normal running conditions no such issues were observed and found to be working fine.
Could you please suggest the possible reason for the reset?