Dear all
1. What is the maximum value of input current limiting that can be set? Is it set by the resister, so I can set infinity value in theory ?
2. Without DPM(dynamic power management), if the input power supply is effective, the output current is directly equal to the input current, and the current value is not limited?
3. Can the output current of Vsystem be up to 6A? The current of Vsystem without battery, only from input of adapter.