Hi,
I'm using LM2734 to design a power supply. The input voltage is 9V and the output voltage is 3.3V. When there is no any load, the output voltage is 3.3V. But when I connect 3 LEDs (about 10mA) to the output, the output voltage diminishes to 2V. I refered to the application on page 25 in the datasheet. Please refer to my schematic as attachment.
Could you please help to check my schematic? Is there any problem?
Thanks.
Kevin Xiong