This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: Switching stop at during startup

Guru 11170 points
Part Number: UCC28740


Hello E2E,

In during startup, if primary current peak is over VCST(max), does UCC28740 stop switch?

Regards,
ACGUY

  • Hi,

    I would not expect the controller to experience VCST(max) during startup because the controller will limit the primary peak current amplitude to 0.63*Ipp(max) when it is in startup mode.If the OCP threshold is exceeded (1.5V on CS pin), a UVLO reset and restart should occur.

    Best Regards,
    Ben Lough
  • Hello,

    Thank you for reply. Please see the attached file. Those are waveform at startup for our board.
    When Vout reached to near 5V, controller is stop switching.
    Is the switching stop trigger Vfb?
    Is this caused by a low crossover frequency?

    Regards,
    ACGUY

    UCC28740 Startup.pdf

  • Hi,

    Thanks for the waveforms. It looks like the device is exiting the soft start sequence (which it should) and then operating in CC mode at maximum Vcs as the output voltage rises. It does appear there is a little bit of overshoot in the output voltage when switching stops. At the moment when switching stops, do you see the VDD voltage get discharged to the UVLO threshold?

    Best Regards,
    Ben Lough
  • Hi Ben,

    I took waveforms. Please see file. Vdd was not drop to UVLO when switch stop.

    My opinions are follow;
     - Vfb rose to over 880mV.
     - Increased Ifb to more than 20uA.
     - fsw decreased to about 170Hz.

    I think the excessive rise in Vfb is due to the OV of Vout. So I thought that this switch stop was the OVP of Vout.

    Countermeasure;
     - Suppress collector current for photocuppler.
     Is it correct?

    Please let me know your opinion.

    Regards,
    ACGUY

    UCC28740 waveform.pdf

  • Hi,

    If you do not see a fault response on VDD then yes, I would suspect excess opto-coupler current is causing the device to stop switching and suppressing the collector current would help. Are you able to share a schematic for this design? Adjustment to the compensation parameters of the feedback loop may also help.

    Best regards,
    Ben Lough
  • Hi,

    Thank you for your cooperation.
    I do like to send you a schematic in private messarge. I will send you a friend application so please approve.

    Best regards,
    ACGUY