This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 85
Part Number: TPS62065-Q1
Hi team,
This is Jessica. glad to work with you.
i have a question about our TPS62065-Q1 design. As the datasheet described, the output L need to be 0.7uH to 1.6uH.
#1 if it possible for customer to use 2.2uH for their design(Vin=3.3V; Vout=1.8V; Iout=0.8A)?
#2 If it is because a larger L will cause the phase margin too low or for any other reasons for that we limited the L range?
Thank you very much for your time.
Best regards
Jessica
____________________________________________________
TPS62810-Q1 – New Automotive 6Vin, 2.25MHz buck family with 1% accuracy and SYNC-pin. 1-2-3-4A options. Smallest 2x3QFN package with wettable-flanks for optical PCB inspection.
In reply to Tanvee: