This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS62065-Q1: Consult for L selection about TPS62065

Intellectual 1270 points

Replies: 2

Views: 84

Part Number: TPS62065-Q1

Hi team,

This is Jessica. glad to work with you.

i have a question about our TPS62065-Q1 design. As the datasheet described, the output L need to be 0.7uH to 1.6uH.

#1 if it possible for customer to use 2.2uH for their design(Vin=3.3V; Vout=1.8V; Iout=0.8A)?

#2 If it is because a larger L will cause the phase margin too low or for any other reasons for that we limited the L range? 

Thank you very much for your time.

Best regards

Jessica

  • Hi Jessica,

    I would recommend to use parameter suggested in datasheet because it is tested. The device would be stable with 2.2uH inductor but output cap and for different LC value feed forward cap should be calculated accordingly. The app note will give detail information about external component selection for stability and feed forward. www.ti.com/.../slva441.pdf ,
    www.ti.com/.../slva289b.pdf

    Best regards,
    Tanvee

    ____________________________________________________

    TPS62810-Q1 – New Automotive 6Vin, 2.25MHz buck family with 1% accuracy and SYNC-pin. 1-2-3-4A options.
    Smallest 2x3QFN package with wettable-flanks for optical PCB inspection.

     

  • In reply to Tanvee:

    Hi Tanvee,

    Thank you very much for your help.

    Best regards
    Jessica

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.