This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21732-Q1: UCC21732 Production Availability

Part Number: UCC21732-Q1
Other Parts Discussed in Thread: UCC21521, UCC21732,

Hello,

I have been using UCC21521 as part of a high power SiC boost converter.  It is working well but it requires a fair amount of external circuitry for optimal use with SiC FETs.  I see TI is coming out with gate drivers with more built in features geared towards the SiC market such as UCC21732.  I will be moving to the next rev of my board and would like to move to this chip or a similar one, but I am hesitant without knowing at least a rough time frame of when the part will hit initial and full production.  Is this information available?  Thanks.

  • Hello Tim,

    Thanks for your interest in UCC21732-Q1! You are correct that there are many additional features for protection which are very useful and necessary for SiC power devices. We typically do not release production information on "Preview" products on this forum. I will connect with you via private messenger with additional details.

    Regards,
    Audrey