Other Parts Discussed in Thread: INA821, UCC24612, UCC24610
In SNOU140A on the app of LMG3410 circuit you have C8 .
This is powering the chip in boost-up mode, shown to be 47uF
This is huge!
In an app where everything is low power, there is low current including peaks.
Can it be selected to something nominal such as 1uF/25V MLCCor something such as 2.2uF?
Is the 47uF value due to the buckboost negative bias the chip generates internally?
Will appreciate a range of values min to max.
Pl see attached pdf of my circuit in 380V @ 300W application where we need 2 such sync switches. I only copy the relevant part of the circuit.
r