Other Parts Discussed in Thread: TL431
We are designing an SMPS (36V/8A) using UCC28600D. We used Webench design tool for the reference circuit. The input given is 220V AC. The problem we are facing is that the output voltage is fluctuating between 9V - 36V. The input voltage given to the IC UCC28600D is also varying from 9V-12V and hence the output pin of UCC28600D is giving a burst of 128Khz pulse. I am attaching the schematic and the waveform of the voltage at VCC pin of UCC28600. What would be the reason for the voltage fluctuation?