This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: About the question when two TL431s are connected in series.

Part Number: TL431

Dear support member,

My customer used TL431.

I have a question.

(Question1)
Is it possible to use two TL431 connected in series to make 2.495 × 2V?

(Question2)
If it make 2.495 × 2V possible,
could you teach if there is something like a recommended circuit?


Best regard.
Bob Lee.