Hello,
I designed a board using the LMR33630ARNXT in the inverting buck mode to generate -9V from a 24V supply and I am seeing issues when power is cycled and the output capacitors are not discharged.
On initial power up with everything discharged the inrush current is a quick spike as expected but when power is cycled and the inrush current peaks to 3.5A for ~25ms causing a supply rated for 3A to enter over current protection.
Swapping to a supply rated for 5A the power rail comes up but the large inrush current is still seen when powering VIN without discharging the Output capacitors.
The EN pin was tied to VIN so the device starts up when the VIN rail reaches ~2V (LMR33630A undervoltage lock-out threshold), could this be the issue?
I am not sure why there is a difference when powering the board with the output caps discharged vs charged.
Thanks,
Sean