Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hello,
I am using BQ27542-G1 and STM32L4+ microcontroler using I2C to manage my Li-Polymer Battery,
I have to update Some BQ parameters according to my Battery settings, theses parameters are :
#define BQ27542G1_DESIGN_CAPACITY_VALUE (0x0960) /* 2400 mAh */
#define BQ27542G1_DESIGN_ENERGY_VALUE (0x2198) /* 8600 mWh */
#define BQ27542G1_DESIGN_VOLTAGE_VALUE (0x0E74) /* 3700 mV */
#define BQ27542G1_V_AT_CHG_TERM_VALUE (0x1068) /* 4200 mV */
#define BQ27542G1_TERMINATE_VOLTAGE_VALUE (0x0BB8) /* 3000 mV */
#define BQ27542G1_CHARGING_VOLTAGE_VALUE (0x1068) /* 4200 mV */
#define BQ27542G1_OT_CHG_VALUE (0x01C2) /* 450 0.1°C */
#define BQ27542G1_OT_DSG_VALUE (0x0258) /* 600 0.1°C */
Based on linux drivers available under this link ( http://www.ti.com/tool/bq27xxxsw-linux) I have developed my own code source that allows me to:
- UnSeal Data Flash memory and Verify Control Status register
- Read Data memory Block (using DataFlashClas, DataFlashBlock, DataFlashData and DataFlashChecksum Commands)
- Verify Checksum value
- Update data Buffer with my proper value
- Write Data memory Block (using DataFlashClas, DataFlashBlock, DataFlashData and DataFlashChecksum Commands)
- Seal Data Flash memory and Verify Control status register
- Soft reset the BQ.
To verify that parameters are correctly stored into my BQ, I read only data memory flash (in Unseal access Mode) and It was equal to what I wrote.
Then, When acquiring BQ data, such as Remaining Capacity (command 0x10) or Full Charge Capacity (command 0x12 ),some acquired data are wrong, like :
RAAC(0 mAh) , VOLT(4116 mV), RARC(0 %), TEMP(26.1 *C) , AS(0 %), FULL, (0 mAh), IAVG(-45 mA)
Note that, after modification registers, when reading the control status registers, all these bits are set to '1': [QEN], [RUP_DIS] and [LDMD]
After that, I modified my defines declared above in order to reset the default configuration as described in the User manual, and the problem still persist!
Finally, I compared the whole data block that I modified (Subclass ID 48, 82, 80, 34, 02) in two different BQs, the first with modified parameters and the second without any block modification, and data blocks are not similar ! there are another fields that are not the same, and not modified using my code source.
Note that I Have to update these parameters using STM32 through I2C and not using BqStudio.
So, My questions are:
- Apart from steps that I described previously, Is there a missing step for writing data flash?
- Is it normal that I found some Data Block fields changed that I didn't set ?
- Is these dependencies between parameters that I have to Set? Did I miss some parameter that I have to update ?
Best Regards,
Ghada,