Part Number: BQ25703A
Other Parts Discussed in Thread: TUSB322, TPS65987, BQ25703
Hello,
I have an application and I wanted to see if the BQ25703A fits.
I need a 12V 2Amp DC supply to power a load. I need that supply to come from a 3S LiIon battery.
I also want to be able to use USB C to charge the battery, preferably while still operating the load, but not a deal breaker.
My questions are:
1) When there is no power adapter or USB plugged in, can the BQ25703A use its' buck/boost to regulate the battery to 12V to supply the load?
2) When USB is plugged in, can the BQ25703A use the 5V-20V USB input and it's buck/boost to supply 12V to the load AND supply the variable voltage to charge the battery?
3) If the USB source is just a normal USB 2.0 low current port or a USB 3.0 port, dedicated charging port, USB C port, or USB C PD supply, does it know, or can I tell it what the USB source is capable of? If the USB port can not supply enough current for the load and charge the battery, I would like to turn off the load and have it just charge the battery.
I will have a host MCU on the board as well to do the USB C power negotiation. But if the USB 2.0 or 3.0 port is plugged in, I do not have USB communication, and therefore can not enumerate to ask for more power.