Part Number: BQ25606
Other Parts Discussed in Thread: BQ24266
As Jacob pointed, if the battery is not connected and you keep the CE low, the VSYS keeps jumping from 3.7V to 4.2V as it sees the BAT as 0V. Is there any way to prevent this without manually enabling and disabling the CE pin ?
For example, if BAT is below 2V, you don't enable charge mode. Is it possible inside the component ? without external discrete components ? Because as I used the BQ24266, it does behave the right way, not like the new BQ25606.
Thanks.