This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CSD95378BQ5MC: Comparison with the CSD95378BQ5M

Prodigy 490 points

Replies: 1

Views: 68

Part Number: CSD95378BQ5MC

Hi,

A customer of mine is using already the CSD95378BQ5M in a design. They wonder what are the main differences with the CSD95378BQ5MC?

Can they use the CSD95378BQ5Mas a direct replacement for the CSD95378BQ5M?

Thank you in advance!

  • Hi JuMar,

    Thanks for the great question!  The CSD95378BQ5MC has enhanced top-side cooling compared to the CSD95378BQ5M.  Electrically they will behave identically.  But the thickness of the two devices is slightly different.  This may affect assembly onto the PCB and mounting of a heat sink if one is used in this application.  Please check these two items and as long as they are ok there should be no issue.

    Regards,

    Evan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.