Hello,
I am using TPS62742 for a battery operated circuit. The battery is single cell lithium thionyl chloride rated at 3.65V. My output voltage is 3.3V with a maximum output current of 150mA.
Is 3.65V input voltage a safe range for such an application?
I am asking because, in the datasheet (typical application circuit), the input voltage range is 4 -- 5.5V for a 3.3V load. However, in several graphs and from the Webench application circuit, a delta of 350mV is permissible.
Please let me know if such a system would work or is prone to failure.
Please find attached my reference schematic.
Thanks PWR_Management.pdf
TPS62742DSSR |