Part Number: TPS62242-Q1
Hello,
I am interested in using the TPS62242-Q1 to power an IC that needs 1.2V +/-5% input. I am trying to determine if the voltage ripple on the output of the TPS62242-Q1 will violate that. Equation 5 in the datasheet tells how to calculate voltage ripple:
Following that equation, I calculated a ripple of 5.185mV when Vout = 1.2V, Vin = 4V, L = 2.2uH, F = 2.25MHz, Cout = 10uF, and ESR = 0.025 ohms.
However, it is my understanding that this equation is only applicable when the device is operating in PWM mode. Since it looks like the ripple in PFM mode will be worse, I'm interested in calculating that as well. The datasheet talks about a PFM comparator threshold and an on-time that it turns the switch on for, but does not mention any specific time. Can someone offer some guidance on how I can predict the maximum voltage ripple in this use case?
Thanks!