Hi ,
While referring to the TPS3808 reset timing diagram on Page 7 of datasheet, require the following clarifications.
In the design VDD is set to 3.3V and VIT is 1.2V.
1.Should the VDD be Vddmin(1.7v) before VIT+hys (sense threshold)
2.Is it Ok for VDD to be 3.3V within the reset duration. In the design when sense reaches VIT , VDD does not reach the 3.3V.
3. Once VDD is >1.7V and then Reset logic depends on VIT. Once sense pin crosses VIT , then there shall be user configured reset delay independent of Vdd and VIT power rails. Please confirm.
4.Does the MR pin accept pulse of 100ns. In datasheet it is mentioned as 1ns (min) . Please confirm.
Your quick response is highly appreciated.