This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: low voltage with no load , 700mS delay when 20amp load applied.

Part Number: LM25119

Hello.

I am having a coulpe of issues with the LM25119.

I am only using 1ch from the chip for now and have disabled CH2.

Running at 50khz Vin18V , Vout 12V. Max output current 25amps.

Issue 1 -  I power up the reg with no load,  and the Vout is 4volts. And the FET is getting pulses very slowy. Once you connect a load (400mA) the reg come to life and Vout is 12V. 

Issue 2 - With reg running a light load, When I connect a 20amp load , Vout drops down to 4volts and after approx 700mS the reg kicks back into life and supply's 12V and 20amps.

Has anyone come across these issues before?

Regards

Steven