This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5017: isolated 15V DCDC PWR supply

Part Number: LM5017

Hello,

my customer is currently designing an isolated PWR supply for their gate driver and is looking at using the LM5017 for this.

Here are the specifications of their 15V DCDC:

Vin: 16 – 30Vdc

Vout min = 16.5V (to be used with a low cost LDO to get a stable 15V)

Vout max: around 20V to limit losses in LDO

I out: 0.3A max

To do some quick testing, they mounted their transformer (i prefer to send share the transformer details offline) on the EVM AN-2204.

They  got an output voltage by connecting in serial both secondary windings of the transformer.

Because they are not comfortable with their first test, They would like to ask you if you could have a look and confirm that it is possible to reach their specifications with this LM5017 and their transformer.

Or if it is preferable to use another dedicated transformer.

thanks for you support.

Regards,

Stani