Other Parts Discussed in Thread: EV2400, BQ34Z100EVM, , BQSTUDIO
Hi,
I'm trying to use a 12V 2.3Ah Lead-acid battery with the BQ34z100EVM and EV2400.
Following the Step-by-Step Design Procedure in the BQ34Z100-G1 datasheet on page 50.
Step 1:
- Design Capacity: 2300mAh
- Design Energy: 2300mAh * 12V = 27600 mWh
- Cell Charge Voltage Tx-Ty: 2300mV
Step 2:
- LED_Comm Configuration: default
- Alert Configuration: default
- Number of Series Cells: 6
- Pack Configuration: VOLSEL bit set
On the BQ34z100EVM the following jumpers are set:
- J5: >5V
- J2: 16V
- J3: A
- J6: EXT
- I2C: connected
Step 3:
- Voltage Divider: (300000+16500)/16500 = 19182
- Flash Update OK Cell Volt: 2800mV * 6 * 5000 / 16000 = 5250 mV ("Value is beyond maximum value defined for parameter")
Then it says "Use the Evaluation Software to calibrate to the applied nominal voltage; for example, 24000 mV."
In bqStudio v1.3.90 I go to Calibration
Tick the Calibrate Voltage box
Fill in 12890mV (measured at BAT+ and BAT- screw terminals)
Calibrate Gas Gauge
"Calibration - Cell Voltage correction is beyond allowed range."
What am I doing wrong? The gauge reports a voltage of 2208 mV
Thanks,
Remko