Other Parts Discussed in Thread: LM5145, LM5161, LM5160
Hello,
I am trying to convert LM5145-EVM to a fly buck converter. I have replaced its inductor with a toroid. I measured the efficiency on the secondary side without loading the primary and its not good, is in the range of 60%-70%. Is it because my toroid has a single turn and is incurring a lot of core loss??
I have used diodes on the secondary side for rectification. I am thinking of driving Mosfet on the secondary side by using the low side gate drive pulse coming from LM5145 and isolating it from the primary by using a small transformer. Is it a good idea??
Any suggestions??
Regards,
Nayana Soni