Hello,
I am using LM1117 for powering micro-controller my design with input 5V from SMPS and output of LM1117 set at 3.3 V. I also have GSM module on same 5V rail with different regulator. I have observed on the oscilloscope that at particular interval when GSM is transmitting the data, both 5V and 3.3 V droops by 0.4 V which causes reset of one of analog IC operating at 3.3 V in my design as it has narrow range of input voltage. I am using 10 uF tantalum capacitor at the o/p of regulator. How can this voltage drop be avoided ?