Other Parts Discussed in Thread: TPS2373, PMP20859
Hi,
Customer has some questions about the oring application on TPS2373-4VM:
1. On TPS2373-4EVM-758, if the pass FET is turned off by APD pin, Adapter would power the system.
The DCDC output would break off, when switching from adapter to PSE. Is it right?
2. The PSE side still keeps connecting since MPS function in TPS2373 would turn on, is it true?
Datasheet shows the MPS would work if APD is higher than 1.65V.
3. If item2 is true, why it can’t switch back from adapter to PSE to achieve smoothly switch between adapter and PSE ?
Can you give some comments about the oring application?
Thanks.