Other Parts Discussed in Thread: TPS53681
Tool/software: WEBENCH® Design Tools
Dear
I need know if is possible make a Circuit with a Constant Current Output using the TPS53467? For example: if the load have very small resistive value and request up than of 100A but i need give only 80A of Constant Current, is possible set the circuit configuration from Pinstrap or NVM for get a precise and constant current output?. Thanks