Hello,
I wanted to understand the calculation of cell balancing time for EM1402 board with a fixed balancing current of 2A .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I wanted to understand the calculation of cell balancing time for EM1402 board with a fixed balancing current of 2A .
I have a pack of 3 LGHG2 cells with capacity of 3000mAh with their respective voltages as 3.525V, 3.428V and 3.622 volts. I want to calculate the cell balancing time for cell 3 to reach to the average value of voltage, which is 3.525V.
Hi Radhika,
Ok, but you will still need to do your own characterization based on your cells to do conversion from mAH to voltage, this is unrelated to the device.
Regards,
Taylor