Other Parts Discussed in Thread: GPCCHEM
Hello everyone,
I contact you because we observe a strange behavoir: at some point the "Remaining Capacity" register increases during a discharge (without change for FCC register).
Here a curve of "DSG_10min_BQ2" file:
Remarks :
- We discharge every 10 mins 2A for 7s.
- Similar behavior had previously been observed (inversion of the remaining capacity). The cause was writing a negative value in the "Cc Delta" register. But the behavior was constant. In our case, what is strange is that it seems to be done in a hazardous way.
For another battery, the voltage drops (there is a short discharge every day for months) and the SOC doesn't follow a logical behavior.
Vbat lower vs SOC higher...
Date |
VBatt |
SOC |
T°C |
flag_status (0x0E/0F) |
05-04-2019 11:00:05 |
23.88 |
100 |
38.4 |
0x0280 |
05-04-2019 11:00:09 |
23.724 |
100 |
38.4 |
0x0281 |
08-04-2019 11:14:34 |
23.898 |
86 |
21.9 |
0x0180 |
23-04-2019 16:22:02 |
23.832 |
92 |
22 |
0x0180 |
24-04-2019 11:01:10 |
23.796 |
93 |
39 |
0x0180 |
The curve :
Our customer and ourselves do not understand this behavior. Can you explain it?
Best regards