Dear all,
Could you give me some advice about the following content?
Our customer ask the cause of phenomena like below.
Our customer measure value of Vref with the circuit below
※Rsup=910Ω, R1=130Ω,R2=120Ω, C1=4700pF, CL=1μF Vsup=+24V
measurement value : Vref=2.457V, 2.454V, 2.460V, 2.452V、2.453V
specification value: Vref=2.483V~2.507V
As understood from above value, measurement value is out of specification value's range.
So, I would like to advice about cause of above content.
It would be great if you could let me know your thoughts this cause.
Best Regards,
Y.Ottey