Other Parts Discussed in Thread: TLVH431, TL431, TLV431
Hi everyone,
I don't understand how feedback work in the evaluation board UCC25630-1EVM-291. I don't have the ev. board to measure voltages or currents so I post this question.
When the output voltage is regulated at 12V the current that pass through the LED of the optocoupler is about 1.45mA. With the assumption that CTR is 100%, the opto collector current must be 1.45mA. From the datasheet the FB current is 85uA and FB voltage must settle at 5.4V so the 1.45mA sink from the collector where it came from?
Is it possible that every time the output voltage goes a little bit up the set point, the FB voltage will drop and the system goes in burst mode?
Thanks for the support.
Filippo.