This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 139
Part Number: REF3312
We have a question about the output current of REF3312. In the data sheet on page 1, is said that this output current is +-5mA
And on page 5 is said that it is +-30mA
What is the actual value? 30mA or 5mA?
Thanks in advance.
If you think this response answered your questions/concerns, please click the button to let us know!
In reply to Abhinav.Sharma:
In reply to user5895002:
Dear Abhinav.
Thank you very much for your reply. Could you tell us the value of this dropout? so, we could know if we are able to support it, You have tested up to 30 mA.
And in case of driving 10mA, the value of the quiescient current is known? Should you mind telling this value to us?
It's very important for us to drive 10mA, in other case we'd have to look for another component.
Mercedes
user,
While we don't have a value or characterization for this dropout exactly, you can see the graph here:
That being said, you can probably extrapolate this data to 10mA to be around 200-300 mV, but this spec can not be guaranteed because it is not characterized. We also do not have the quiescent current value, this is another spec that would need to be tested. Since 10mA is still technically within our operating conditions, The Iq shouldn't be outside of the spec in the datasheet.
Thanks,Abhinav.