Hi Support,
Currently our products use TI's Load Switch and DC-DC to implement Power's part.
However, there are problems that find that the voltage drop is very large. Therefore, I would like to ask if the IC solution we choose is suitable and whether there are obvious problems with the circuit diagram design.
The attached part is the circuit diagram of this part.
At present, our general situation of Power's Solution is as follows. We find that there is a voltage drop between VCC_3V3_HOST and VIN, and the voltage drop increases as the current rises.
Test data is as follows.
In addition, in the TPS22975 Datasheet, on page 6, it is mentioned that RON at IOUT = -200mA means that if the back load is large, the Load Switch will generate a large voltage drop?
Thanks.