Other Parts Discussed in Thread: TPS22901, , TPS22912C
i understand that when the device is on that it takes 500mA typical to trigger the RCB circuit. However, when the device is off, what are the conditions for reverse blocking? I want to wire OR two of these devices and one will always be on and the other always off. One has a Vin = 3.3V and the other 1.2V. I'm currently using a TPS22901 and getting reverse current flow which is causing the circuit to fail. Ideally, i'd like to replace the TPS22901's with a footprint compatible device. Note that this is urgent as I need to get working boards to my client in 2 days.
Thanks.