Customer is asking for replacement device to APL5930 in PC applicaiton.
APL5930 has ±1.5% over Line, Load, and Temperature Range.
I am checking TPS74901 with 2% accuracy. Is there any other suggestion? Cost is also one concern. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Aki,
Yes the TPS74901 is one option to consider. I would also look at TPS7A84A as another option, especially if output accuracy is a concern (TPS7A84A offers 0.75% accuracy across line, load, and temperature).