This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54233: Started with A load of 1.5A, but the output voltage is only about 2V

Part Number: TPS54233

Hi Guy;


        I have a problem; Started with A load of 1.5A, but the output voltage is only about 2V;Could you tell me what the problem is; thank you!


The following test was done;


1. It can be started normally under light load, and can work normally when the load is increased to 1.5a when the power is on;

2. After power supply, the switch between no load and loaded 1.5a can work normally;

3 if the defective board is replaced with a good IC, it can work normally and the undesirable phenomena will disappear;Replace again undesirable IC, phenomenon appears;The impedance of bad IC and good IC is almost the same.

4. Test the waveform of defective plates;Operating frequency: 300KHZ/8,Vsen< 0.2v;Comply with the characteristics of overcurrent protection described in the specification;Now suspect may be in the boot, IC overflow protection phenomenon

schematic diagram