Hi team,
I have a question with TPS2547 Status pin when feeding back to customer's questions.
My customer wants to use the status pin to realize a feature to boot the system the first time if the current drawn from 2547 power rail is larger than 300mA.
I suppose this can be realized by regulating the ILIM_LO setting right?
But also seems that there is still another current threshold as 45mA and 55mA for the load detect also works and change the Status pin level. Could you help to explain to me how the status pin is triggered please?
If the 45mA/55mA is the threshold? Or any situation that the ILIM_LO and the 45/55mA are separately used?
Thanks for your help
Max