Hello,
Let me confirm about below.
* According to datasheet DC spec, when user will use TPS3702C with ""SET" pin = High".threshold is set to "+/-4%".
In addition, accuracy of threshold is +/-0.9% at over temperature condition. So, worst case will be "+/-4.9%" in this case.
However, according to "Table 2 Design parameters" in datasheet, this shows "+4.94%/-4.86%" as worst case.
The question is
--
* I understood that condition of "Design result" of "Table 2 Design parameters" is measurement value.
In this case, VSENSE measure "3.30132 V", so worst case become "3.30132 * 1.049 = 3.4630(4.94% of "3.3V")" and "3.30132 * 0.951 = 3.1395(4.86% of "3.3V")".
Is my understanding correct ?
--
Best Regards,