This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62140: TPS62140: Could I leave VOS pin unconnected

Part Number: TPS62140
Other Parts Discussed in Thread: TPS62147, TPS62148,

Hi team

I need to get a 3V to 12V programmable output voltage with 2A capability using TPS61240;

1, Why output voltage of TPS61240 is limited within 0.9V~6V?

2,I want to trim the FB pin to adjust the output voltage with following method, so I want to leave VOS unconnected, just use FB pin。Can I do this? If not, reason is?

many thanks!