Part Number: TPS54335A
Hi
My customer has question.
The usage conditions are as follows.
VIN = 27 V
Vout = 5V
IOUT = 40 mA
When used under the above conditions, a phenomenon occurs in which the resistance value between PH and GND decreases (about 5 Ω).
I saw this article, is the same phenomenon occurring?
If so, please cooperate as we would like to respond promptly.
Regard
T Kishi